Hi Team:
since TMP451 has one I2C slave address, if customer use three parts, so how to configure their I2C address? thanks!
*******************************************************************************************************************************************8
7.5.1.3 Serial Bus Address
To communicate with the TMP451 device, the master must first address slave devices using a slave address
byte. The slave address byte consists of seven address bits, and a direction bit indicating the intent of executing
a read or write operation. The TMP451 device has a device address of 4Ch (1001 100b). Additional factory programmed
device addresses are available upon request.