Hi team,
I was wondering if you could help with the following question about a specification in the TMP100-Q1 data sheet (SBOS581A –SEPTEMBER 2011–REVISED MAY 2017).
In section 7.5 Electrical Characteristics under Temperature Input, the parameter “Accuracy (temperature error) vs supply” is listed at a maximum +/-0.5 °C/V. What is the reference voltage for this parameter? The device is specified “At TA = −55°C to 125°C and V+ = 2.7 V to 5.5 V” and I am operating it at -47°C to 87°C and at 3.3V.
Thank you in advance for your help!
Errol