Other Parts Discussed in Thread: AWR1843
I am developing a radar board using IWR1443 radar chip with the out-of-box demo code. Everything is working fine with the out-of-box demo code. I then add the group tracking algorithm in the main code. The final code size is around 160K and it cannot not be compiled.
I then take out some of the unused modules in OOB and shrink the program code. I could incorporate the group tracking algorithm (~\mmwave_sdk_02_01_00_04\packages\ti\alg\gtrack) into the OOB within 128K. However, the code stop at the first line of code in the gtack as shown below. This statement eventually will call the Memory_alloc() function which will involve the heap memory. Just wonder if the heap used by the gtrack is the same as the heap assigned for the radar L3_ram. Do I have to assign a different heap for gtrack?
Also want to know if there is demo code other than the OOB which incorporates the gtrack algorithm already.
Thanks,
Henry