Other Parts Discussed in Thread: IWR1443
Hi,
I have an IWR1443 module, It is working fine. I would like to enquire regarding the units which are showing in the y-axis of the time-domain plot> It shows 'codes', I am not sure what that means. In my understanding, it should be some voltage. I require to plot the magnitude of the signal which is (I^2+Q^2)^.5, so what would be the unit of the x-axis and y-axis if I am plotting only one chirp with 256 samples. Kindly advise me on the same.
Many thanks,
Sruthy