This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Download firmware over SPI by external MCU

Part Number: AWR1243

I used the DFP tool to run the mmwavelink_example  and found the trace.txt file. Is it the SPI command that drives AWR1243? If so, I plan to add some delays to each instruction in order. Use an external MCU to write the SPI instructions in trace.txt into 1243 through SPI, so that there is no need for mmwavelink porting. Is this feasible? 

Looking forward to your reply.

Sincerely

x Peter