Hello,
Would like to know the Short circuit current linearity of OPT101 will be able to measure at 340nm. For our application we are looking the intesity upto 10^-14 lx and expect about 10 piccoampere for that intensity
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Would like to know the Short circuit current linearity of OPT101 will be able to measure at 340nm. For our application we are looking the intesity upto 10^-14 lx and expect about 10 piccoampere for that intensity
Hi,
Linearity is spec'd for device voltage output. Can you clarify here?
Best,
Alex
Sorry for delay in response, My query was actually to understand if the output of the photodiode is linear upto 1 picoampere ie., can it measure the light intensity less than 10^-12 watts/M^2 intensity
Hi Dilip,
The datasheet indicates: "The photodiode is operated in the photoconductive mode so the current output of the photodiode is very linear with radiant power throughout a wide range. Nonlinearity remains less than approximately 0.05% for photodiode currents less than 100-μA." However this is a very low light level and we do not have data down to this level so I am not able to say if this will be the case at this low of a light level.
Best,
Alex
Hi Dilip,
The dark current of this device is 2.5pA and will also increase with temperature as stated in the datasheet. This would be a major source of error with such low light levels and result in bad linearity.
Best,
Alex