Other Parts Discussed in Thread: LDC1001, , TDC7200
Hello there,
I would like to compare here LDC1101 and LDC1001 in LDC DRDY Timing measurement.
All based on SNOA941A App Report and LDCs manuals SNOSD01D and SNVSBF7.
I want to use LDC1x01 for high resolution and fast sample rate (10 kSPS).
I have tested LDC1101 with 15 mm dia coil which has resolution 2 um with RCOUNT 5A (90 usec).
Base on this experiment I believe that increasing timing resolution (1/16e6 = 62ns resp. 1/32e6 = 31.125ns based on SNOA941a header 3) will increase also resolution of the sensor.
Important aspects I am aware of:
A1: LDC1001 can use only 8 MHz reference oscillator compared to LDC1101 with 16 MHz which I do not think it is important in case of LDC DRDY Timing measurement since LDC works as even counter.
A2: LDC1001 can drive sensors 5kHz-5MHz compared to LDC1101 0.5-10MHz. Depending on application an appropriate LC tank may be chosen.
A3: LDC1001 has compared to LDC1101 INTB functionality on special pin (16) which gives advantage for MCU using it instead of getting it from SDO as on LDC1101.
A4: Sensor amplitude for LDC1101 is 1.2Vpp compared to 1-4 Vpp by LDC1001.
A5: LDC1101 is approximately half the price.
Q1: What LDC can give higher performance in DRDY timing mode? (if not comparable based on A1)
Q2: LDC1001 should be capable of driving bigger inductor since it can drive smaller Rp (800Ω --> 4000kΩ) compared to 1.25kΩ to 90kΩ by LDC1101, correct?
Q3: Is the LC tank driver stronger by LDC1001? Is it important?
Q4: If DRDY Timing measurement is set, LDC1101 set in LHR mode will not measure any Rp correct? (The measurement stability is not influenced)
Q5: Is the sample rate achievable in this measuring configuration same for both?
Thank you very much for your answers.
Best Regards,
Michael