Hi,
In 3D People Counting, a watchdog is added, but the callback function of the watchdog is not included. The following is the initialization function of the watchdog, please help me to have a look. thank you
void mbRadar_watchdogInit(void) { Watchdog_Params watchdogParams; /* Initializa the Watchdog driver */ Watchdog_init(); /* Initialize the Watchdog driver default parameters */ Watchdog_Params_init(&watchdogParams); gWatchdogInt = 0; watchdogParams.resetMode = Watchdog_RESET_OFF; watchdogParams.callbackFxn = watchdogCallback; watchdogParams.debugStallMode = Watchdog_DEBUG_STALL_ON; watchdogParams.windowSize = Watchdog_WINDOW_100_PERCENT; /* texp = (DWDPRLD + 1) x 8192 / RTICLK. if RTICLK = 200MHz then 255 means 10.5ms .*/ watchdogParams.preloadValue = 255; watchdogParams.socHandle = gMmwMssMCB.socHandle; watchdogParams.esmHandle = gMmwMssMCB.esmHandle; /* Open the Watchdog driver */ watchdogHandle = Watchdog_open(0, &watchdogParams); return; }