Other Parts Discussed in Thread: HDC1080
Hello,
the datasheet mentions the following:
«Reduce prolonged exposure to both high temperature and humidity extremes that may impact sensor accuracy.”
Could you quantify what is meant by:
1) prolonged - how long?
2) high temperature and humidity extremes - the sensor is specified with 0-100% and -20...125°C. Where are the limits for high temperature and humidity extremes
For our application: Could we measure temp and humidity at -20°C to 80°C without any damage to the sensor and any loose of accuracy )outside the tolerance from the diagrams)?
Thanks and kind regards,
Alen