Part Number: DRV425EVM
Other Parts Discussed in Thread: DRV425, TIDA-00463
I am researching methods for building a magnetometer for conducting geophysical surveys to detect buried ferrous objects such as pipes or cultural items such as iron tools. These items can be detected using a conventional proton precession or fluxgate magnetometers and have field strengths which are typically greater than the earth magnetic field by 500 to 25,000 nano Teslas (i.e. 50,500 to 75,000 nT total). For conducting surveys, logging of the total magnetic field at around 50 to 200 readings per second would be ideal. Also, averaging of readings measured at higher rates (i.e., 1000 Hz averaging 5 readings to arrive at 200 averaged readings per second) to hopefully reduce noise would be helpful. The sensor would be placed around 2 feet above the ground surface for collecting measurements while moving the instrument around the areas of interest.
Is the DRV425 sensor capable of sensing sizable ferrous objects 2 feet above the ground at total field magnetic field strengths of 50,500 nT and at 200 Hz sampling rate?
If I read the information correctly, the TIDA-00463 module would use 2 DRV425, and is equipped with instrument amplifiers and analog to digital converters (ADC). Does TI plan to build a TIDA-00463 or similar item?
If not, would the configuration of the TIDA-00463 work as a geophysical instrument sensor for use as described in my first question and are the specified amplifiers and ADCs sufficient to reduce noise and increase the sensitivity or are better components available?
Thanks
Jim Major