Hi team,
I found that "7.5 Electrical Characteristics" says tPD typical value is 12.5us. Could you tell me your comment for lower questions?
a) "8.3.4 Propagation Delay" says "The first graph shows the typical case. The magnetic field goes above the BOP value at the moment where the output is updated. The part will then only need one cycle of tPD to update the output.". Does it mean its actual propagation delay is tPD=12.5us?
b) "8.3.4 Propagation Delay" says "The second graph shows a magnetic field going above the BOP value just right before half of the sampling period. This is the best case possible where the output will be updated in just half of the sampling period". Does it show its actual propagation delay is 0.5*tPD=6.25us? In addition, why the best case is before "half" of the sampling period? Does it mean the least sampling time to update update is 0.5*tPD?
b) "8.3.4 Propagation Delay" says "Finally, the third graph shows the worst possible case where the magnetic field goes above the BOP value just after half of the sampling period. At the next output update, the value will still see a value under the threshold and will need a whole new period to update the output." Does it indicate its actual propagation delay is 1.5*tPD=18.25us?
Regards,
Ochi