Part Number: TIDEP-01000
Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843ISK, UNIFLASH, IWR6843
Hi Sir/Madam,
Based on the people counting and tracking reference design, I bought the IWR6843ISK and MMWAVEICBOOST. Based on the instructions for hardware setup of ICB for flashing mode and the instruction for flash the mmWave Device, it always have an error when I load the flash image. The information is shown below:
All steps I set for the device followed the instruction and I am sure I chose the correct number of COM. I also restarted the device to re-flash.
One thing I am not sure is that the Uniflash can detect my device as MMWAVEICBOOST when i open it. But i cannot start with that.
Based on the instruction, i chose the device in new configuration section and chose the device IWR6843ISK. It happened that errors.
In addition, i also want to try to choose the device MMWAVEICBOOST, but it doesn't have this device in the new configuration in UniFlash.
I have been stuck here for a long time, do you know what is the problem happened here?
Many thanks in advance!
Sensen Xing