Hi,
I am Yonghee Lee and working for LG innotek as a software engineer in motor control.
I am supposed to use LMT87 as a temperature sensor and I would like you to tell me the real maximum operating range of LMT87.
According to the LMT87 transfer function, the range of operation is from -50 to 150, or from 538mV to 3277mV when it comes to accuracy.
I am wondering if the sensor keeps working on even when voltage out is out of the maximum range shown in transfer function,
In addition, I want to know the real maximum range of the temperature and voltage out that can be measured regardless of transfer function in the datasheet.
Please let me know if you can and feel free to leave the comment about this question.
Thank you.
Best Regards,
Yonghee Lee