This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

IWR1642: How to run mmw demo if customer can't access Internet

Mastermind 29985 points

Replies: 7

Views: 2773

Part Number: IWR1642

Hi,

Some of my customer can't access Internet in their company. So they can't try the out of box demo (mmw demo) at office.

Can we provide other option to customer to run the mmw demo without Internet?

Thanks,

Thanks,

Chris

  • Hello Chris,
    They can try downloading the offline version of the demo visualizer from the following link : https://dev.ti.com/gallery
    and search for “mmWaveDemo Visualizer”. There is a download option there.

    Regards,
    Vivek
  • In reply to Vivek Dham:

    Vivek,

    I download a file named mmWave_Demo_Visualizer for windows as you suggest in below link, but how to run it? I change it to exe file and it doesn't work in win7.

    Thanks,

    Chris

  • In reply to Chris Meng:

    Hello Chris,
    Once you download the file "mmWave_Demo_Visualizer.zip" , unzip this to a location on your PC. This would have an executable "mmWave_Demo_Visualizer-1.0.0.setup-win_4.0.0.exe" to setup and install the visualizer utility , follow the instructions that pop up.
    Once its installed it would show up in your windows programs and you can run it.

    Regards,
    Dham
  • In reply to Vivek Dham:

    Vivek,

    The file I downloaded has no suffix. After I added zip as suffix, I can unzip it. I will try it when I am back to office next week.

    Thanks a lot for your help!

    Thanks,

    Chris

  • In reply to Chris Meng:

    Vivek,

    When I installed the mmWave_Demo_Visualizer-1.0.0.setup-win_4.0.0.exe, it asks to install GUI composer runtime on-line or from local file.

    As customer can't access Internet, we need to find the off-line installer for it.

    I only found we can download GUI composer runtime v1 at below link, but in install_image_mmWave_Demo_Visualizer.zip, I found install_image_mmWave_Demo_Visualizer\mmWave_Demo_Visualizer\docs\GUI_Composer2_Release_notes.html which says the version of Runtime version number: 3.0.0 and it should be v2.

    Where can we download GUI composer runtime v2 installer for mmWave_Demo_Visualizer?

    Thanks,

    Thanks,

    Chris

  • In reply to Chris Meng:

    Hello Chris,

    Can you try installing GUI Composer using the following .exe? This is the same version of GUI Composer that I have on my PC.

    gcruntime-4.0.0-windows-installer.exe

  • In reply to aozer:

    Aozer,

    It works though the install of Visualizer failed at first time. But I reinstalled and it works ok then.

    Chris

    Thanks,

    Chris

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.