Hello,
I'm working on a temperature application using TMP275. It works pretty well.
In the datasheet, it is said accuracy is +/-0.5°C ( form -20°C to 100°C, V+=3.3V, with a 12bits resolution ).
But I cannot find out this result form the "TEMPERATURE ERROR vs TEMPERATURE" curve ( page 4 ). Where the accuracy seems to be +0.125, -0.200 from -20°C to 100°C.
So I'm confused,....
Do I misunderstand this curve ?
In fact I'm looking for TMP275's accuracy and repeatability from 0°C to 40°C.
And is there any linearity problems ?
Thanks
P.A.M