Other Parts Discussed in Thread: LDC1612EVM, LDC1612
After installing the "LDC13xx16xx EVM GUI" software on a Windows 7 machine, I plugged in the LDC1612EVM. The software does not connect. After searching the device manager, I found that the LDC1612EVM was connecting as a "USB Input Device". I tried to update the driver manually by right clicking the device and selecting "Properties>Driver>Update Driver". I browsed to the "C:\Program Files (x86)\Texas Instruments LDC13xx16xx EVM GUI\driver" directory but after selecting "Next" Windows says the "USB Input Device" is the best driver.
Then I searched the forums and found that the same story existed for LDC1000 and that flashing the firmware helped for the LDC1000 (with the respective GUI and firmware version).
But in my case the same approach (flashing the LDC1612 firmware) did not help. The PC still attaches the EVM as USB Input device.