Other Parts Discussed in Thread: LMT87, LM94022
Hello all:
Searching around on the internet (including TI forums), I can't seem to find a definitive answer to my question:
I'm using an LM34DM (SO-8) in "minimal" configuration: connections to +5V, GND, and Vout to a PIC18 ADC pin.
Datasheet tells me Vout is 10mV/degF, which is what I'm getting at "normal" temps (above 0F). If temperature falls below 0F, will LM34DM Vout fall below GND? (I'm not equipped to test temps this low).
I'm using the LM34DM to have the PIC take action at a threshhold temperature (200F). Works great. But I'm anticipating deployment of my circuit in Midwest U.S. where temps can fall far below 0F in winter. I have two concerns:
1. ADC input much more than a small amount (0.3V) below GND may damage the PIC.
2. Vout below GND might cause the PIC ADC register to 'wrap' around to a spurious high value above my threshhold.
The answer I "want to hear" :-) : Vout never falls below GND.
Thank you for any assistance.
-Mike