This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC2256A: DDC2256A about VIH and VIL issues

Part Number: DDC2256A

Hi team,

The customer is using DDC2256A along with Xilinx Artix 7 FPGA. The datasheet shows the min VIH is 0.8DVDD and the max VOL is 0.2DVDD. That is if DVDD is

1.8V, the min VIH is 1.44V and the max VOL is 0.36V.  But FPGA cannot meet these two values.

Q1: Is there any ways to solve this issue?

Q2: The datasheet  also shows the differential output voltage(VOD) is 700mVpp. But the maximum differential input for Artix 7 FPGA is 600mV. 

Is there any ways to solve this issue?

Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments