Part Number: FDC2114
Other Parts Discussed in Thread: , LDC2114
Re: FDC2114 and waveform seen on the sensor inductor and sensor.
Referring to the datasheet Section 9.1 sates “to an oscillation of a LC resonator” which I assume means a sine wave.
Referring to the datasheet Figure 13, this drawing shows a sine wave for the activation, settling, etc periods.
I quote from just after Table 9
“The CHx_IDRIVE field should be programmed such that the sensor oscillates at an amplitude between 1.2Vpk (VSENSORMIN) and 1.8Vpk (VSENSORMAX). An IDRIVE value of 00000 corresponds to 16 µA, and IDRIVE = b11111 corresponds to 1563 µA” Which again I assume means a sine wave.
A sine wave, I do not get. I see only the positive half of a sine wave the negative side is stuck at 0 volts. This looks as if the the waveform has passed through a rectifying diode.
Please note this is NOT something I have done wrong. The effect is in my development FDC2114 system AND In T.I.s unaltered FDC2114EVM evaluation module.
I believe it is not the connection of the scope causing this. I have treated the sensor as a RF radiator and "received" the waveform without making an galvanic connection to the FDC circuit.
My Questions: Is this normal and not a sine wave or is there a special way to view the waveform developed in the FDC? If it is not a sine wave and is of a rectified nature how is this for EMC radiation? Does the set up of the "1.2 ~ 1.8 volts pk" drive current need clarification due to it being an asymmetrical wave?