This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

IWR1642BOOST: TIDEP-0090 - Built .bin File NOT Running

Prodigy 210 points

Replies: 5

Views: 836

Part Number: IWR1642BOOST

Hie guys 

So after  getting help from TI, I managed to build  Traffic Monitoring Object Detection and Tracking Reference Design and generated a .bin file.

I programmed the IWR1642 chip successfully but Immediately after power-up the hardware fault led goes on and no messages are coming on the serial port.

I also noticed that the .bin file that comes with the demo project also does not run

I have managed to run the demo in the debug configuration only.

Please help

  • Hello Leslie,

    The current TIDEP-0090 was meant to be run via CCS load mechanism and so the bin file will have to be recreated.

    In order to try out to do so a minor change to makefile would be needed to work with mmWave SDK1.0

    I am attaching the modified makefile that should help you create the bin file and for reference I am attaching the bin file created with this makefile.

    Please try it out and let us know if you continue to see any issues.

    Attachments:

    TMdemo_changes_0717_SDK1.0.zip

    Thank you,

    Vaibhav

  • In reply to Vaibhav Mahimkar:

    Hie Vaibhav

    Thanks will try it out. 

    Regards

  • In reply to Vaibhav Mahimkar:

    Hie Vaibhav

    The makefiles are identical, what has changed ?

    I includes the same makefile for the cortexr4 and the dsp

    Regards
  • In reply to Vaibhav Mahimkar:

    Hie Vaibhav

    My apologies.

    It worked now the bin file is running.

    Regards
  • In reply to Leslie Guyo:

    Hi Leslie,
    No worries, happy to help.
    Hope you were able to notice the makefile difference in the final bin creation step.


    Thank you for verifying the answer.
    Please file a new ticket if you need further help.

    Vaibhav

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.