This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE58JD16: How to use the PN?

Expert 2655 points

Replies: 1

Views: 419

Part Number: AFE58JD16

Hi team,

    My customer has some question about the IC, Could you give him some advice?

1.   NM1~INM16 are NC ,should I connect them to ground or VCC with a resistance?

2、ADC_CLKP &ADC_CLKN are LVDS, Should I add a 100 ohm to short out?

3、In datasheet(Rev 0.5  Mar/2015  )P113  Figure38   VREF_IN_REXT is connected with a cap ,Why do this ? And I don't find the Pin. As the yellow part:


4、Is DGND apart from AGND? AVSS1.8V is apart from DVSS1.8V? Do you have some recommendation about  decoupling capacitor?

5、FCLK & OUTPUT DATA have wrong position? Is FCLK equal to F_CLKIN? Is Data Rate equal to N*F_CLKIN ?

1 Reply

  • Hello,

    We have received the query about the device AFE58JD16.
    Since AFE58JD16 is an NDA restricted device, I would like to take the conversation offline.
    Please send an email to praveen.aroul@ti.com

    Regards

    Praveen

    TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.