Hi
Below is my questions about TMP302.
1. TMP302 maximum output current is 10mA, in which conditions?
2. I want to drive TMP302 with VRTC, VRTC maximum output capacity is 2mA, when system is shutdown, consume 0.1mA, can 1.9mA meet TMP302 operating normal?
3. Does TMP302 have power dissipation only when it trigger the temperature point, and what is the maximum power consumption? In normal conditions, is there only 15uA power consumption?
Thank you