Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443
Hello,
I have written some python code that reads data from the IWR1443 BOOST EVM and interprets it (while the mmwave demo is running),
I have been wondering if I can set this up on a Linux machine, specifically a small arm based Linux machine. The issue I have been having is that without the emupack the serial ports cannot be found and the version of this software for Linux seems to be precompiled for an x86-64 Linux setup.
My main aim is to get data from this EVM to a raspberry pi or other board so that it can be embedded in a mobile platform for a prototype robotics project, is this at all possible?
Could the IWR1443 DEVPACK be used to this end at all?
Thank you for your answers,
Dexter