Part Number: AWR1642
Hello,
I have some issue as my title.
i find the power of two Tx antennas cannot be changed at the same time.please look the fft graph below:
i had changed the back-off code of Tx to 30, i think it means both Tx1 and Tx2 should be reduced 30dB at the same time,
but the changing only show at channels of Tx2. Levels of Rx5-Rx8 are lower than max power 30dB,but Rx1-Rx4 not changed.
My configfile is below:
-------------------------------------------------------------------------------------------------------------
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg 0 0 1 1
profileCfg 0 77 7 7 58 30 0 68 1 128 2750 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 32 0 400 1 0
lowPower 0 0
guiMonitor 1 1 1 1 1 1
cfarCfg 0 0 8 4 4 0 5120
cfarCfg 1 0 4 2 3 0 5120
peakGrouping 1 1 1 1 255
multiObjBeamForming 1 0.5
calibDcRangeSig 0 0 20 32
sensorStart
-------------------------------------------------------------------------------------------------------------
Is there something wrong? Please tell me the way to change the power of two Tx at the same time.
Best Regards;
Duan