Hello,
From the trace log file from the AWR1243 BOOST set up, and from the AWR ICD,I noticed that the host sends the 0x5678 0x8765 0xFFFF .... 0xFFFF message on the channel.
This message signals that the host is ready to receive the messages from the AWR SPI slave device. Is this message necessary for the communication protocol to work since the host is always the master and the AWR is always the slave ?
Is this message only necessary if we enable ACK based messaging ? If I do not want ACK based messaging (which I can enable from the command message flags), then can I get away with not having the host to send this 0x5678 message ?
Thank you
RJ