Hi Team,
Can you confirm which one of the below two statements in datasheet are correct when remote sensor is not being used in remote sensing?
Page 13:
When not using the remote sensor with the TMP461 device, the D+ and D– inputs must be connected together
to prevent meaningless fault warnings
Page 23:
The TMP461 device requires only a transistor connected between the D+ and D– pins for remote temperature
measurement. Tie the D+ pin to GND if the remote channel is not used and only the local temperature is
measured.
Regards,
Praveen