Dear TI Support,
I am currently working with the following HW chain: AWR1243BOOST + DEVPACK + TSW1400, and the following SW chain: Radar Studio v1.9.2.1 + HSDCPRO. Currently, I am able to capture the raw ADC data following the standard procedure given in the user guides, i.e., setting up the radar parameters using Radar Studio -> Setting up the TSW1400 -> ARM TSW1400 -> Trigger Frame. Finally, with the resulting .bin/.csv file we are able to post-process the data using our own MATLAB scripts. However, our intention is now to make this entire capturing/post-processing automatic.
I have gone through the documentation on Lua Scripting for Radar Studio and, as far as I understood, by using the LUA Schell, we can automate Radar Studio completely. However, I am still not able to understand how can I link or control Radar Studio through another program like, for example, MATLAB. Is this possible ?. Currently, there is a way already to link MATLAB with HSDCPRO. I wonder if there is also a similar procedure to link MATLAB with Radar Studio? If it is possible, is there anyway that someone can give me a hint or just a starting point for this?.
Thank you in advance for your response.