Part Number: MMWAVE-DEVPACK
Other Parts Discussed in Thread: IWR1443BOOST
Hi,
I am trying to get the RadarStudio data capture to work. I am following these slides here:
The problem I am encountering is that the drivers will not install. This occurs for all four ports.
I have tried restarting the computer and the same error occurs. Repowering the DevPack and IWR1443BOOST resulted in the same result. Also tried using the old dfp version "C:\ti\mmwave_dfp_00_07_00_04\rf_eval\ftdi", and the the ftdi folder included with the sdk package, "C:\ti\mmwave_sdk_01_01_00_02\tools\ftdi", and same problem has occurred. I have not tried it on a different machine. Here is the hardware setup:
I did not alter any of the jumpers on the mmWave DevPack. 4 of the LEDs are on: DS7, DS6, DS5, DS3. Also, DS1 is faintly on. Please advise.
Sincerely,
William Tran