Part Number: LDC1614EVM
Other Parts Discussed in Thread: LDC1614, LDC1314
Hi,
I have revamped the LDC1614 to fit into our application, I finally have the hardware up and running.
I noticed that when I flash it, my board version and the OneUI application show connected, but it thinks it is connected to : SSP EVM connected - LDC1314.
I've verified that the LDC1614 is populated on the board.
Also if I try to update firmware via USB-BSL, the USB connection drops immediately and never upgrades to the package I need, the pcb starts a loop of reconnecting and dropping but it does this at different times during the update. (FET is disconnected while doing this) and the red led on the board is on, I do hear the USB connecting to system and see it in the EVM in windows device manager.
Any ideas/suggestions?
Thanks.