Part Number: IWR1443BOOST
I have issues with CFAR engine in IWR1443BOOST. I want to do peak detection on complex input data (to do log2 and magnitude inside the CFAR)
If I correctly understood from previous CFAR threads here, in that case, data format after magnitude and log2 operations in CFAR engine will be Q7.11.
Is that mean that threshold needs to be in Q11 format? So, in mmwDemo it was in Q9 format and it was 1024 so I need just to set it to 4096?
In mmwDemo for xWR14xx before CFAR detection, log2 results from all virtual antennas are summed so does this sumation impacts the formula for
calculating detection threshold like in xWR16xx case (number of virtual antennas taken in consideration)?
Best regards,
Predrag