Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443
Hello,
So I posted this question a week ago and got one reply and since then nothing so I am going to try this another time and hopefully someone will have some answers for me.
I am trying to get the fps of the radar higher using the mmwave visualizer but it crashes every time, here is what I tried:
- I put the antenna config on all antenna's, set the fps to 20, lowered the range resolution to 0.04 and the range to 7.17, I did uncheck the grouping for range direction and checked the remove static clutter and I only checked the scatter plot. for this configuration the module crashes immediately and I see this error in the visualizer: mmwDemo:/>Exception: ../main.c, line 1726.
As I found another thread, this one here: e2e.ti.com/.../2325812 it stated that it was not supported to set the fps higher, but as I am not using the heatmap and only the scatter plot I can not see anything related to that. It also stated that the UART can't keep up with the data as the fps are set higher. So I tried to modify the demo code so it should send less data. I made it so that when it would send the data in stead of the whole package I just tried to send 1 byte, but this didn't make any different and it still crashes.
I tried using the same configuration with different antenna configurations:
- 4Rx and 2Tx, it runs for like 10 seconds and i see some data on the visualizer but after a short while it still crashes.
- 4Rx and 1Tx, it runs! and it seems like it is working with this configuration. Only when I put it up to 30 fps it seems that after a minute or so it crashes again.
So as I tried to send less data through the UART I feel like that isn't the problem, could it be that when using all of the antenna's the processor can't keep up with all of the calculations and then crashes?
I also want to say that I need to use the elevation antenna so the first configuration I did is what I need. If someone could clarify if there is a known issue with this and if there is a possible way around this that would be nice. As long as I get some answers on this I would be happy and less stuck on this matter.
Thank you,
Vera