This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC6821: Application: FAN speed control abnormal

Part Number: AMC6821

Hi there:

Our customer would like to do FAN speed control (ex: 100%, 90%, 80% or else...) , when 100% speed control, it’s OK;

but when in 90% speed control, we found some issue as following

Each PWM output signal with about 680ms interval. register set in DCY control mode. 

Or any suggestion we could check from register viewing? 

Question 1:

Does this 680ms interval case an normal symptom? 

Question 2:

When zoom-in the PWM waveform, we found 2 different duty frequency; Does that normal happen in one PWM output?