This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

If mmWave sensor can penetrate an object?



Dear Sir

I want to scan an object inside structure. The object around 3-5cm and contained high moisture. Is there any mmWave sensor can penetrate of this object. 

Please advise.

Thanks

  • Hi

    Theoretically FMCW can penetrate through structures. It can detect objects in rain/snow and hence moisture shouldnt be a problem. It should also be able to detect 4cm objects easily.

    But practically, it depends on lot of physical parameters, like reflectivity of the intruding structure, how far the sensor is placed, reflectivity of the Object etc.
    It also depend on the Antenna design and the emitted waveform. Another thing to consider is whether the object is moving or stationary. How strong is the clutter in the environment also affects the detection capability.

    In short, It should be able to detect in your usecase but unless more specific details are available, it cannot be accessed.
  • Thanks Santhana
    Can I have you contact details? I will discuss with you more.
    My email is hong.zhang@agresearch.co.nz
    Thanks