Part Number: OPT3101
I read the OPT3101 datasheet and the "Introduction to Time-of-Flight Optical Proximity Sensor System Design" app note, and I'm still wondering how LED's with different radiant intensities and FOV will affect max range of the system. For example, the LED used in the app example was the SFH 4550 with radiant intensity of 1100mW/sr and FOV of 6 deg, but the SFH 4650 has an equivalent output power of 180mW, but only a radiant intensity of 90mW/sr and greater FOV of 30 deg. I did not find any equations in the app notes/datasheet that take this into account when computing max range, but I'm new to optics and TOF, so maybe I missed something.