Part Number: AWR1642BOOST
Other Parts Discussed in Thread: MMWAVE-SDK, , SYSBIOS, AWR1642
Tool/software: Code Composer Studio
Hi,
I am new to this, but I am having trouble loading the following files through Code Composer's Studio. After creating the Target Configuration file. The ccxml file isn't in a Target Configuration list, and when I right click it I can't find the option to Launch Selected Configuration.
Is this document up to date? I had to go back to mmWAVE SDK 1.1 in order to run this capture demo.
4. 4. 3. 2. Connecting to xWR14xx/xWR16xx EVM using CCXML in CCS
Follow steps in above section to create a ccxml file. Once created, the target configuration file will be seen in the "Target Configurations" list
and you can launch the target by selecting it and with right-click select the "Launch Selected Configuration" option. This will launch the target
and the Debug window will show all the cores present on the device. You can connect to the target with right-click and doing "Connect
Target".
Best Regards,
Jeff