Part Number: AWR1243
Hi team,
I have a customer asking about the correct gain value using in AFE.
As we known, The RX gain is the gain of the complete RX chain, including LNA, VGA.
For example, If we get 0dBm at before ADC. And the Rx Gain is set to 30dB, RF Gain Target is set to 26dB.
Does it means the signal input from RX pin is 0-30-26 = -56dBm?
Is the RF Gain Target means the 77GHz LNA Gain before 77GHz Mixer?
Thanks,
Regards,
Wesley