Dear TI Team,
I would like to use the component PGA460 in the following application:
Measuring range 0.3 - 8m (with a horn)
I have tested now different transducers and reach 8m very well. But I cannot measure below 0.38m. The damping resistor has already been adjusted. And I have adjusted amount of pulses and current.
I have now removed the R36 and soldered a second (same) transducer to J14 (SLAA733 - point 4.4.5).
I can't pick up an input signal at the GUI/data monitor now.
In monostatic operation, the transducer "cracks" audibly in the Hertz range. Nothing can be heard in bi-static mode.
The following questions:
Is there anything else to consider in theschematic or GUI?
Does it need a receive only sensor?
If I reach 0.38m with a mono-static solution, what is the minimum distance that can be achieved with a bi-static solution?
I know it depends on the transducer, but would 10% less distance be possible?
Thank you.