This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LMT87-Q1: LMT87-Q1 External lead plating thickness

Prodigy 455 points

Replies: 1

Views: 170

Part Number: LMT87-Q1

Hello

Can you please clarify what is the correct thickness of external lead plating of LMT87QDCKRQ1?

i have heard two different numbers: 50 to 150 microinches (μm) or  5 - 20 μm. Which one is correct?

Piotr Demidowicz

 

  • Piotr,

    The mechanical information is located on pg 21 of the datasheet. It appears that the lead thickness is 150 um.

    -Kelvin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.