This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT87-Q1: LMT87-Q1 External lead plating thickness

Part Number: LMT87-Q1

Hello

Can you please clarify what is the correct thickness of external lead plating of LMT87QDCKRQ1?

i have heard two different numbers: 50 to 150 microinches (μm) or  5 - 20 μm. Which one is correct?

Piotr Demidowicz