Hello,
I am trying to read data from AWR1243 using RadarStudio. I have connected all the hardware correctly (AWR1243BOOST+DEVPACK+TSW1400) and I am following the instruction given in the "RadarStudio's UserGuide.pdf". However, I am not able to open the Radar Studio Application as it is throwing a "Object Reference not set to an instance of an Object" error. The same error is being thrown when I try to open "mmwave studio" application as well. I am using Windows 10 with 64 bit operating system. I tried uninstalling HSDC Pro and reinstalled it and then tried opening Radar Studio GUI. But still it gives me the same error. Could anyone help me on this? What can I do to rectify this issue?