I was wondering if it is possible to set 4 or 5 occupant zones for Occupancy Detection demo (I’m using Automotive toolbox 1.2.0). I tried changing the zone definition in the chirp configuration as,
“zoneDef 4 13 16 9 15 13 16 27 15 40 16 9 15 40 16 27 15” to set 4 zones but I’m getting an error (from both Matlab script and executable GUI) that maximum zone limit reached. Can someone please help me to increase the number of occupancy zones to 4 or 5?