Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1443, IWR1642, DCA1000EVM
Tool/software: TI-RTOS
Hi,
Now, we have IWR1642 and IWR1443 EVMs and we want to save raw ADC data from demo visualizer. But now, we receive point cloud data from data-port UART and get the real-time plots. Is it possible to get raw ADC data from data-port UART and then get real-time plots in demo visualizer?
I still have some specific questions:
1. Is it possible to receive both raw ADC data and point cloud data at the same time via data-port UART? or we can only transmit one of them via the data-port UART?
2. If it is possible to receive raw ADC data via data-port UART, can we process it in real-time in demo visualizer? since the UART speed limits to 1Mbps.
Thank you.
Best regards,
Jiadi