Part Number: IWR1443
Other Parts Discussed in Thread: MMWAVE-STUDIO,
Hi,
My customer would like to know the generic development flow of IWR devices especially RF and DFE configurations.
For example, one of my customer is seeing the following whitepapar

And found the Table 2. Chirp configuration and radar performance for fluidlevel sensing. It seems this describe the target performance for this specific application.
My customer`s questions is --- How to define the spec for the specific application and how to implement the configurations into the target device ?
As for former question, should we use mmWave Sensing Estimator ? If so, how to import the configurations into mmWaveStudio or target device ?
And as for latter question ... it is difficult for me to explain, but I`ll try:
I know the environment of IWR devices + DCA1000 with mmWaveStudio can be used to evaluate RF/DFE performance with various configurations (Too many configurations ! -- and many parameters are unclear to use...). I think this environment would be useful to evaluate RF/DFE performance in early development phase, but once the configurations are validated, how can user implement these configurations into their own IWR firmware ? In case of IWRxxxBOOST + DCA1000 environment, we use binary image for IWR firmware and unfortunately, there is no source code for that. In other words, the communications (control and commands between mmWaveStudio GUI and the target IWR device) to configure RF/DFE are still unclear. So even if the configurations are validated on IWRxxxBOOST + DCA1000 environment. I`m wondering if users couldn`t understand how to program the IWR device to have the same RF/DFE performance with IWRxxxBOOST+DCA1000 environment.
I know some source code are available for demos (for example, ppcount, level sense, etc...). All of them are using UART for command I/F to configure IWR device including RF/DFE. Each demo has their own command handler implementation to parse the incoming commands and execute rader APIs. So if we should use the demo sample code as a template for customer`s application, I think it might be useful if we have mapping information from the above black-boxed communication to rader APIs to be executed in the target device.
Could you please kindly suggest ? Please note I`m new in mmWave devices.
Best Regards,
NK