Hi,
We currently developing a device with the tmp116n device, and I have a question regarding accuracy depending on Vcc. In the datasheet, the accuracy is given depending on temperature and power Vcc.
For our application, temperature is pretty stable around 39°C. By now, we planed to power the pcb directly from battery. But now we also take into account using an LDO to reduce Supply voltage down to 1.9V or 2.0V.
Do you have more infomation on accurcy with fixed temperature? Or is the additional error for one-shot conversion (as given in Figure 3) for 2V about -0.02°C, so neglectable?
Thanks for your help.