Other Parts Discussed in Thread: AWR1642
How do i find out the maximum range that AWR1642BOOST EVM can Support?
Also in the formula, Range_Max=IFmax*C/(2*S)
what should be the value of IFmax in 1x sampling mode?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How do i find out the maximum range that AWR1642BOOST EVM can Support?
Also in the formula, Range_Max=IFmax*C/(2*S)
what should be the value of IFmax in 1x sampling mode?
Regards
Hi Rahul,
IFmax is 5MHz in AWR1642. But Since Maximum Range depends on Slope, so lower the slope, larger the maximum range.
Max Range would also depend on other parameters like transmit power, Antenna gain etc. Refer to below link which would give you an idea of how Maximum range can be measured with key parameters.
Regards,
Kaushal