Other Parts Discussed in Thread: INA826EVM, , DCA1000EVM, IWR1443, INA826
I have a IWR1443BOOST connected DCA1000EVM and I am using a INA826EVM as external trigger. The INA826EVM is connected to a USRP N210 and being powered with DC Power Supply. The INA826EVM is connected to my IWR1443BOOST through pins 4 and 9.
I've confirmed that the IWR1443BOOST is receiving a pulse from the USRP and that there is voltage in the wires connecting to the IWR1443BOOST. However, there is no data being sent to the computer from the DCA1000EVM board. The IWR1443BOOST worked just fine when I used a Software Trigger and ran the DataCaptureDemo_xWR. It is only failing me when I began using the Hardware Trigger.
Any suggestions on what I can do?