Hello everyone.
I am trying to build a vehicle tracking system with reference to the traffic monitor lab.
This system must satisfy the following requirements.
· GUI should be built with MATLAB.
· Tracking is done outside the sensor (done on the GUI).
· Use GtrackLib created in C language for tracking.
In other words, you have to make GtrackLib MEX and operate it.
Unfortunately, the following inquiries have revealed that the traffic monitor lab does not support MEXization of GtrackLib.
There is also no plan to support in the future.
e2e.ti.com/.../725819
So, I'm trying to fix it so that PCMex mode of tm_play works.
For that reason, it will be a great help if you answer the following questions.
------------------------------
1.
In the answer to the above URL I heard that "There are two different versions of GtrackLib".
What is the difference between the two versions?
(I need to think about which version I should use)
2.
MEXization of the traffic monitor lab is a recognition that has been completed halfway.
What kind of processing is not implemented?
------------------------------
I am very grateful to you.
Thank you.