Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH, IWR1443, AWR1443, MMWAVE-SDK
Tool/software: TI-RTOS
I was trying to run the demo using mmWave Demo visualizer web app with the IWR1442Boost EVB out of the box. After configuring the ports, an error message reported a mismatch in SDK version 2.1 but device reporting 1.2
I then tried to flash the device per instruction using the UniFlash application and loading the
mmwave_sdk_02_01_00_04/firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin and the
: Meta Image 2/MSS - : mmwave_sdk_02_01_00_04/packages/ti/demo/xwr14xx/mmw/xwr14xx_mmw_demo.bin
This was unsuccessful, with errors stating that the files did not match the correct headers. One of the forum post suggested to only try and flash the Meta Image 2/MSS but this did not work. I then rebuilt the demo application and tried flashing the newly compiled binaries. This also did not work and resulted in the same error message - copied below.
I would greatly appreciate some help and guidance for getting this to work.