This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Why AWR1642 power rail 1.2V cunrrent increase 150mA at high temperature

Part Number: AWR1642


Hi team,

Customer has a question about the 1.2V power rail current.

When testing AWR1642 in 25 deg, the current of 1.2V is 510mA. When testing AWR1642 in 85 deg, the current of 1.2V goes to 670mA, and now the Tj of AWR1642 is 120 deg.

Question: Why the current of 1.2V power rail will increase 120mA at high temperature? Did you have any software solution that can decrease the TJ?

Thanks.

Regards,

Wesley

  • Hi,

    We are checking for similar test with our characterization team

    thank you
    Cesar
  • Hello Wesley,

    150mA current increase at high temperature is completely normal, and similar to what we have seen in characterization.

    The Tj is going to be directly related to the power consumption and the heat sinking capabilities of the board. In order to reduce Tj you will need to either reduce the power consumption of the device or increase the heat sinking capabilities of your PCB/system. You can lower the duty cycle, reduce the number of tx/rx, reduce tx output power, etc in order to reduce the overall device power consumption. We do not have any custom software designed to reduce the Tj, this will need to be done by modifying their sensor configuration and/or PCB.

    Regards,

    Adrian
  • Hi Adrian,

    Thanks for your reply.

    Could you please point out where I can find these description in datasheet?

    What's the current range that's acceptable for each power rail?

    Thanks.

    Wesley

  • Hello Wesley,

    This data is not described on the datasheet and is only part of our internal characterization of the device. We do not have a spec for device current vs temp.

    Regards,

    Adrian
  • Adrian,

    Thanks for your support.