This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: BPM for 3 TX

Part Number: IWR6843

Currently IWR6843 supports only BPM per the post below.

IWR6843 datasheet says

6.3.1 RF and Analog Subsystem
The RF and analog subsystem includes the RF and analog circuitry – namely, the synthesizer, PA, LNA,
mixer, IF, and ADC. This subsystem also includes the crystal oscillator and temperature sensors. The
three transmit channels can be operated up to a maximum of two at a time (simultaneously) for transmit
beamforming purpose as required; whereas the four receive channels can all be operated simultaneously.

Does this means BPM for 3 TX is not supported?



  • Hello,

    The 6843 device supports operating any 2 transmitters at a time so 3 TX BPM MIMO is not supported as it requires all 3 transmitters operating simultaneously.

    Please mark this thread resolved if your question was answered otherwise get back if more support is needed.

    Regards
    -Nitin